Hello guys,
In my current project, I'm using PN7462 module from NXP. I need that module for the following:
1. To communicate with NFC card
2. To communicate with GSM module via UART interface. I need to have 1.8V level UART communication with GSM unit. Configuration commands for GSM should be sent from PN7462 to GSM.
3. To control a few of the GPIO signals.
I'm reading PN7462 datasheet but I'm not sure I can digest it in a way to properly design my board. Would you guys be so kind to help me with the following:
1. How to supply the PN7462 module? Which power pins do I need to connect to power supply? How to achieve 1.8V for UART and GPIOs?
2. How to download the firmware on PN7462? Using SWD interface ?
3. How to properly design the antenna circuit for NFC communication. Is there any antenna chip available on the market or I need to print it on a PCB?
Thank you very much for your time and effort. Really appreciate it.
Looking forward to reading from you.
Sincerely,
Bojan.
 
					
				
		
 Kan_Li
		
			Kan_Li
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Hi Bojan,
Please kindly refer to the following for details.
1. How to supply the PN7462 module? Which power pins do I need to connect to power supply? How to achieve 1.8V for UART and GPIOs?
-PVDD is used for pad voltage reference and supply of the host interface (HSU, USB, I2C, and SPI) and the GPIOs. so if you use PNEV7462B , you may connect PVDD to an external power, please also note in such kind of case, If PVDD is externally supplied, the Jumper 42 (PVDD_OUT) needs to be set. By setting this Jumper the PVDD_OUT is shorted to GND and the PN7462AU turns off the PVDD LDO.
2. How to download the firmware on PN7462? Using SWD interface ?
-Yes, exactly.
3. How to properly design the antenna circuit for NFC communication. Is there any antenna chip available on the market or I need to print it on a PCB?
- You may find all you need from the following link: http://www.nxp.com/docs/en/application-note/AN11706.pdf
and yes, PN7462's HSUART just supports slave mode, so you have to use GPIOs to simulate a UART interface by software. Sorry for the inconvenience that might cause.
Hope that helps,
Have a great day,
Kan
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
:smileyhappy:
Hi guys,
By reading a PN7462 datasheet, I noticed that it has a high-speed UART which can operate in slave mode only. What actually does that means?
Will I be able to control GSM module through that HSUART in a way to send AT commands from PN7462 and to read the response of GSM module?
Thanks,
Bojan