NXP TagWriter - contact vcard - phone error - version 4.8.3.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP TagWriter - contact vcard - phone error - version 4.8.3.

6,302 Views
t_kubicek
Contributor I

Hallo 

I discovered error in vcard format when writing the phone value as business card in NFC chip either from from QR code 3.1: vcard typ copy. As result of this there is some error in format copany and as result of this when encoded, it is not possible import the contact after tapping the phone.

Is there any update soon to solve this simple bug?

Please also advice how to create correct csv template for writing multiple business cards eg. 200 pcs

See my template trial attached.

t_kubicek_1-1623742775793.png

Thanks for answer

Tomas 

0 Kudos
Reply
7 Replies

6,184 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Dear Tomas,

My apologies for this, I realized that the problem resides in the way the vCard NDEF is being created by our TagInfo app from a QR Code. Thank you for the bug report, I already addressed a ticket. Unfortunately, I'm not able to give you a date for an app update with this issue fixed.
I don't know If you have checked the following document where VCard NDEF is explained along with an Excel example.

https://inspire.nxp.com/tagwriter/tag-writer-user-manual.pdf 

As you might be able to realize, in section 6.2 where the datasets template is shown, specifically in the fourth subsection; Each Colum should have a field from the card information. This .csv file should be copied to your phone memory and by that way, you would be able to write each entry in your Tag. This is more explicit in the NFC TagWriter User Manual from the link above.

Thank you for letting us know about your findings and share them with the community, we appreciate the effort.

Best Regards,
Fabian
0 Kudos
Reply

6,169 Views
t_kubicek
Contributor I

Hallo Fabian,

In the first submitted request for this topic you can find my csv template in zip file created based on your manual. Could you please check it and correct this.

Unfortunately it does not work and it is not clear where I did mistake. Thanks Tomas

0 Kudos
Reply

6,158 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello,

At this moment we are having troubles with the vCard NDEF creation from .csv files by using our TagWrite App. In order to create different types of NDEFs, you are welcome to use our App or, the TagXplorer tool for Windows available in the next link.

https://www.nxp.com/products/rfid-nfc/mifare-hf/mifare-desfire/tagxplorer-pc-based-nfc-tag-reader-wr...

I'm sorry for the problems this issue might cause We are trying to fix this as soon as possible.

Best Regards,
Fabian
0 Kudos
Reply

6,225 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello Tomas,
I hope you are doing well, my apologies for the late response.
I've successfully created the vCard based on a .csv file with the following structure:
====================================
BEGIN:VCARD
N:Smith;John;
TEL;TYPE=work,VOICE:(111) 555-1212
TEL;TYPE=home,VOICE:(404) 386-1017
TEL;TYPE=fax:(866) 408-1212
EMAIL:[email protected]
ORG:Smith Designs LLC
TITLE:Lead Designer
ADR;TYPE=WORK,PREF:;;151 Moore Avenue;Grand Rapids;MI;49503;United States of America
URL:https://www.smithdesigns.com
VERSION:3.0
END:VCARD
======================================
As you are able to see, the version of the vCard is 3.0 and after creating the QR code for this structure and scanning it with our TagWrite App, the fields are created successfully. I recommend you to use this version and you shouldn't have any problems.

Best Regards,
Fabian
0 Kudos
Reply

6,220 Views
t_kubicek
Contributor I

Dear Fabian, until this step was all fine also on my side.

Nevertheless when I try to tap the encoded NFC tag, the phone was not included in the phone. 

It looks the same Tel format mistake is also in your code. 

Please send me the csv file and the QR code. I will test it on my device. 

Thanks

Tomas

0 Kudos
Reply

6,285 Views
Fabian_R
NXP TechSupport
NXP TechSupport

Hello Tomas,

Thank you for using our NXP products, we appreciate your preference.

First, I will recommend that you edit out the sensitive info displayed in the above photo.

Please provide a little more information about the procedure you are following and the NXP tools you are using to write into the NFC tag. Also, the part number of the tag you are using can be known by scanning the Card with our proprietary Android App TagInfo.

Thank you in advance for the answer.

Best Regards,
Fabian
0 Kudos
Reply

6,274 Views
t_kubicek
Contributor I

Dear Fabian, thanks, I eliminated all personal info.

Additional I found out that this happens only when scanning the QR code vcard format 3.0. / 2.1 so the process following: 

1.) Create QR code vcard format (tested 2.1. and 3.0 version)

2.) Scan via NXP Writer QR code copy

3.) Encode into NFC tag

4.) Scan via phone - see NXP info scan above

 

 

0 Kudos
Reply