NXP PN553 NFC Controller driver porting on android 7.1.0 with iMX6D

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NXP PN553 NFC Controller driver porting on android 7.1.0 with iMX6D

5,398件の閲覧回数
danny_lu
Contributor II

Dear Sir/Miss,

 

I have a problem about NXP PN553 NFC Controller driver porting on android 7.1.0 with iMX6D.

Currently I can able to read NFC tag information but NFC module keep sending 3 bytes 61 23 00 every 10 sec as below:

01-01 00:06:45.494 709-862/com.android.nfc D/NxpNciR: len =   3 > 612300

 

And I got this error as below:

00:06:45.494 709-842/com.android.nfc E/BrcmNfcNfa: unknown opcode:0x23

 

Could someone help me to understand why NFC module keep sending 3 bytes?

Please see the full log file in the attached.

Thank you

Danny Lu

ラベル(2)
0 件の賞賛
返信
3 返答(返信)

3,404件の閲覧回数
Yang555
Contributor I
I have also encountered this problem, and have you finally come up with a solution? Thank you.
0 件の賞賛
返信

3,405件の閲覧回数
Yang555
Contributor I

I have also encountered this problem, and have you finally come up with a solution? Thank you.

0 件の賞賛
返信

5,072件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

Regarding "61 23 00" NCI notification, it indicates NFC POLL discovery cannot be performed because of missing TVDD supply.

 

For your information, PN553 is not a mass market product. Please contact local NXP CAS team or local distributor for better support.

0 件の賞賛
返信