NXP PN553 NFC Controller driver porting on android 7.1.0 with iMX6D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP PN553 NFC Controller driver porting on android 7.1.0 with iMX6D

3,133 Views
danny_lu
Contributor II

Dear Sir/Miss,

 

I have a problem about NXP PN553 NFC Controller driver porting on android 7.1.0 with iMX6D.

Currently I can able to read NFC tag information but NFC module keep sending 3 bytes 61 23 00 every 10 sec as below:

01-01 00:06:45.494 709-862/com.android.nfc D/NxpNciR: len =   3 > 612300

 

And I got this error as below:

00:06:45.494 709-842/com.android.nfc E/BrcmNfcNfa: unknown opcode:0x23

 

Could someone help me to understand why NFC module keep sending 3 bytes?

Please see the full log file in the attached.

Thank you

Danny Lu

Labels (2)
0 Kudos
Reply
3 Replies

1,139 Views
Yang555
Contributor I
I have also encountered this problem, and have you finally come up with a solution? Thank you.
0 Kudos
Reply

1,140 Views
Yang555
Contributor I

I have also encountered this problem, and have you finally come up with a solution? Thank you.

0 Kudos
Reply

2,807 Views
jimmychan
NXP TechSupport
NXP TechSupport

Regarding "61 23 00" NCI notification, it indicates NFC POLL discovery cannot be performed because of missing TVDD supply.

 

For your information, PN553 is not a mass market product. Please contact local NXP CAS team or local distributor for better support.

0 Kudos
Reply