NXP NFC Suitability

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NXP NFC Suitability

1,568 Views
doesnotapply
Contributor I

NXP:

We are working on an NFC medical application with the following requirements:

- Reader and Tag antenna coils both PCB loop type 25mm square

- Coils can be accurately aligned

- Coils will be separated by 6-10 millimeters

- Tag will be field powered and will include additional circuitry that must also be powered from the field

- Tag circuitry power consumption varies from a few mW to as much as 70mW

Is this doable as a NXP solutions?

Will a power amplifier be required?

We are leaning towards NFC-B - will the power level allow for effective data communications with varying tag loads and varying separation between coils?

0 Kudos
Reply
1 Reply

1,394 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Daniel

I believe that you can reach your requirement with the PN512

PN512|NXP

And please check the P5DF081 that is part of the MIFARE family.

P5DF081|NXP

regards

Vicente Gomez

0 Kudos
Reply