NTAG5: AREA_1 questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTAG5: AREA_1 questions

ソリューションへジャンプ
211件の閲覧回数
rfid_profi
Contributor I

Hi,

I have several questions about the restricted AREA_1 memory section of the NTAG5 devices:

  1. Is it right, that the read and write passwords are always needed to have access to the AREA_1 from NFC perspective ? That means, you always have to use the SET_PASSWORD Command before reading or writing data to this section, right ?
  2. With the  GET NXP SYSTEM INFORMATION command you can read the PP-Pointer, which divides  AREA_0_H and AREA_0_L. Is there a similar command to read out PP_AREA_1 ? Maybe reading the configuration register  Device security configuration bytes is a solution here, but i don't want the configuration being readable from NFC perspective

Thanks for the answers and best regards !

0 件の賞賛
返信
1 解決策
196件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @rfid_profi

Hope you are doing well.

The SET PASSWORD command has to be executed just once for the related password if the IC is powered.

Regarding PP_AREA_1, you would need to read block 3Fh to get PP_AREA_1 value.

Regards,
Eduardo.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
197件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @rfid_profi

Hope you are doing well.

The SET PASSWORD command has to be executed just once for the related password if the IC is powered.

Regarding PP_AREA_1, you would need to read block 3Fh to get PP_AREA_1 value.

Regards,
Eduardo.

0 件の賞賛
返信