NTAG Boost Antenna Resonance Frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NTAG Boost Antenna Resonance Frequency

485 次查看
joshgott
Contributor I

I am using the NXP antenna design tool in order to obtain parameters for an antenna for the NTAG Boost. I was curious as to why the default Receiver Resonance Frequency was 14.84 MHz as opposed to 13.56 MHz.

0 项奖励
回复
1 回复

457 次查看
Tomas_Parizek
NXP Employee
NXP Employee

Hello joshgott, 

 

The NTAG5 Boost uses "Active Load Modulation", so there is a receiver (LArx, LBrx) path and transmitter path (LAtx, LBtx). It might be quite tricky to tune them exactly at 13.56 MHz. So we recommended keeping the "receiver" path resonance around 14 MHz and the transmitter up to 16 MHz. 

BR

Tomas 

 

0 项奖励
回复