NTAG 424 DNA Interrupted Read Data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG 424 DNA Interrupted Read Data

Jump to solution
1,903 Views
lukas_l
Contributor II

Hi,
I am trying to read the NDEF data file of my factory fresh card. When using the command ReadData with a specified length below 0x7A everything is fine. But with longer length or zero for full file I only get back 122 bytes also missing status bytes.
Card: NXP NTAG424 DNA
Reader: NXP CLRC663+
Status of Card: initialised and authenticated with Key0
Sample: trying to Read full length of File 2
PCD to PICC: 90 AD 00 00 07 02 00 00 00 00 00 00 00
PICC to PCD: 00 00 00 ………. 00 122 bytes overall no Status bytes (expected 256 Bytes Data + 2 Bytes Status)
Really would appreciate any inside.

0 Kudos
Reply
1 Solution
1,861 Views
lukas_l
Contributor II

I found the error. The card only supports frame size 128 bytes in the data link layer and my implementation of the link layer disregarded that.

View solution in original post

Tags (1)
0 Kudos
Reply
1 Reply
1,862 Views
lukas_l
Contributor II

I found the error. The card only supports frame size 128 bytes in the data link layer and my implementation of the link layer disregarded that.

Tags (1)
0 Kudos
Reply