NTAG 424 DNA Interrupted Read Data

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NTAG 424 DNA Interrupted Read Data

ソリューションへジャンプ
1,974件の閲覧回数
lukas_l
Contributor II

Hi,
I am trying to read the NDEF data file of my factory fresh card. When using the command ReadData with a specified length below 0x7A everything is fine. But with longer length or zero for full file I only get back 122 bytes also missing status bytes.
Card: NXP NTAG424 DNA
Reader: NXP CLRC663+
Status of Card: initialised and authenticated with Key0
Sample: trying to Read full length of File 2
PCD to PICC: 90 AD 00 00 07 02 00 00 00 00 00 00 00
PICC to PCD: 00 00 00 ………. 00 122 bytes overall no Status bytes (expected 256 Bytes Data + 2 Bytes Status)
Really would appreciate any inside.

0 件の賞賛
返信
1 解決策
1,932件の閲覧回数
lukas_l
Contributor II

I found the error. The card only supports frame size 128 bytes in the data link layer and my implementation of the link layer disregarded that.

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
返信
1 返信
1,933件の閲覧回数
lukas_l
Contributor II

I found the error. The card only supports frame size 128 bytes in the data link layer and my implementation of the link layer disregarded that.

タグ(1)
0 件の賞賛
返信