NTAG 424 AuthenticateEV2First RndA not matching

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NTAG 424 AuthenticateEV2First RndA not matching

2,399 Views
shaghayeghnz
Contributor II

Hi,

I am currently developing an application using Flutter to write to an NTAG424 DNA NFC tag; however, I am encountering some issues with AuthenticateEV2First. I get the correct response 9100h but my RndA is not matching with the RndA that I generated.

for instance my generated RndA is 13c5db8a5930439fc3def9a4C675360f. The D(K0 , TI || RndA´ || PDcap2 || PCDcap2) is d8e5fa458b297bedbdc3f3d3d81a09b4746b8598fbaf31afd8afc24623eb2e2. As you can see the RndA' does not match with the one I generated.

p.s. My decryption method works correctly with the examples in https://www.nxp.com/docs/en/application-note/AN12196.pdf

Best regards, Shaghayegh.

Tags (1)
2 Replies

1,670 Views
TobiasWeis
Contributor I

Hi, I am having the same problem. Did you find a solution?

0 Kudos
Reply

2,360 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @shaghayeghnz 

Please try the following steps:

Step 1: Field On + RF Reset + Activate Idle + RATS+PPS

Step 2: Originality signature verification

Step 3: ISO SELECT NDEF Application

Step 4: Get File Settings

Step 5: GetVersion

Step 6: AuthticateEV2First ( key store by key 0 = 00000000000000000000000000000000)

BR

kelly

0 Kudos
Reply