NT3H2x11 authentication limit behaviour

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

NT3H2x11 authentication limit behaviour

跳至解决方案
1,507 次查看
Paul_PVS
Contributor I

Hi, I'm designing with the #NT3H2111/#NT3H2211

There is a register AUTHLIM that can be used to limit negative authentication attempts.

Page39 of the datasheet:

8.7.2 Limiting negative verification attempts

To prevent brute-force attacks on the password, the maximum allowed number of negative password authentication attempts can be set using AUTHLIM. This mechanism is disabled by setting AUTHLIM to a value of 000b, which is also the initial state of NTAG I2C plus.

If AUTHLIM is not equal to 000b, each negative authentication verification is internally counted. As soon as this internal counter reaches the number 2AUTHLIM, any further negative password authentication leads to a permanent locking of the protected part of the memory for the specified access modes. Independently, whether the provided password is correct or not, each subsequent PWD_AUTH fails.

Any successful password verification, before reaching the limit of negative password verification attempts, resets the internal counter to zero.

So here is my question:

How permanent is the locking of the protected part of the memory?

Is this "permanent locking" until the device (power-on-)reset ? Or until the next time a NFC-device (smartphone) is presenting itself? 

Or is it really permanent turning the device useless?

I cannot find the answer in the datasheet or AN11786.

 

标记 (2)
0 项奖励
回复
1 解答
1,485 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Paul,

 

Yes, your understanding is correct. After reaching the AUTHLIM, the protected part of the memory will be in a permanent locking, that cannot be reversed.

 

Regards,

Ricardo

在原帖中查看解决方案

3 回复数
1,489 次查看
Paul_PVS
Contributor I

Hi Ricardo,

Thank you for your answer.  Can you then confirm the following conclusion: 

In applications where an accredited user in possession of a valid password must be able to write in the protected memory, the use of the AUTHLIM feature can lead to sabotage through brute force techniques. This would result in the definitive destruction of the device, as the accredited user would no longer be able to use it afterward due to the permanent locking of the protected part of the memory, which cannot be reversed.

Is this correct? (in which case we will not be able to use this feature - a possibility to reset the permanent locking only by the I2C-side would have been the better solution)

Best Regards,

Paul.

 

0 项奖励
回复
1,486 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Paul,

 

Yes, your understanding is correct. After reaching the AUTHLIM, the protected part of the memory will be in a permanent locking, that cannot be reversed.

 

Regards,

Ricardo

1,493 次查看
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hello,

 

Hope you are doing well. As mentioned on the DataSheet, As soon as this internal counter reaches the number 2AUTHLIM, any further negative password authentication leads to a permanent locking of the protected part of the memory for the specified access modes. Independently, whether the provided password is correct or not, each subsequent PWD_AUTH fails.

 

Regards,

Ricardo

0 项奖励
回复