NT3H2111 from RF Detect (Phone)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NT3H2111 from RF Detect (Phone)

1,387 Views
griffith_chen
Contributor I

Hi,

Currently, I use this IC for testing. And on this stage, I can use micro-control through I2C to read/write NT3H2111 in user memory (1 K version), so I implement a function to write NDEF message into user memory, then I use Android phone and turn on NFC and launched "NFC TagInfo by NXP" Application, but the phone cannot detect anything.

So, I want to know 2 questions as following,

1. Does any configuration I need to be set through I2C first?

2. I think even NFC tag has no content, the phone still need to detect the NFC tag, isn't it?

ps. I use same phone to detect other NFC tag product, the phone can detect it, so I think that there has no worry from phone side.

Thank you so much.

Tags (3)
0 Kudos
Reply
1 Reply

1,285 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Griffith,

Could the tag be detected before you write the NDEF data into this device via I2C? Please kindly clarify.

Thanks for your patience!

Have a great day,
Kan

 


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply