NT3H2111 SRAM Mirror

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NT3H2111 SRAM Mirror

1,712 次查看
straga_riccardo
Contributor I

I'd like to write some data from my micro (I2C side) to the SRAM of a NT3H2111. I also want to be able to modify the SRAM via an app on my phone, so I decided to enable the SRAM mirror (SRAM_MIRROR_ON_OFF = 1) and to disable the pass-through (PTHROU_ON_OFF = 0).

I have also chosen 0x01 as SRAM_MIRROR_BLOCK.

My questions are :

1) Is the eeprom endurance go down each time I write on SRAM via I2C ?

2) Is the eeprom endurance go down each time I write on SRAM via the NFC ?

Thank you

Riccardo

标记 (2)
0 项奖励
回复
1 回复

1,533 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

No, the fact that the SRAM is mirrored to the EEPROM means that the SRAM will be accessible to the NFC interface. This way, you will be writing to / reading from the SRAM directly on both interfaces.

For more information, please refer to chapter 8.3.4 of the data-sheet:

https://www.nxp.com/docs/en/data-sheet/NT3H2111_2211.pdf 

Regards,

Ivan.