NT3H2111 Running With 5V

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NT3H2111 Running With 5V

1,094件の閲覧回数
robertosocorreg
Contributor I

Hi,

We have a design that needs to run with 5V Vcc. The microcontroller that talks to the NT3H2111 chip runs with 5V. According to the NT3H2111 datasheet, this chip work between 1.67V and 3.6V. Do you have a chip like the NT3H2111 that works with 5V? We don't want to use level converters or anything like that. We need a simple inexpensive solution. Do you have any suggestions or ideas?

Thank you,

Robert

0 件の賞賛
返信
1 返信

1,013件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 There is the same question with you in case. Please refer to the case and you will receive the feedback via email. Have a nice day.

0 件の賞賛
返信