If we don't need the I2C function and event detect signal for NFC tag application. Can we just connect LA and LB to coil and connect VCC(Pin6) to VOUT(Pin 7). All other pin leave opened. Do we need to add a capacitor to VCC for this application? Besides, datasheet recommended that for energy harvesting a Class 5 antenna is required. What will be the effect if we only have a coil antenna with 9mm diameter