NHS3152 DAC, Single-Shot vs Continuous

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NHS3152 DAC, Single-Shot vs Continuous

2,940 次查看
rcorder
Contributor I

I tried ADCDAC0 example code from the NHS31xx SW API doc:

Example-1 Single Shot Digital-to-Analog Conversion with Polling

   Chip_ADCDAC_Init(NSS_ADCDAC0);
   Chip_IOCON_SetPinConfig(NSS_IOCON, IOCON_ANA0_0, IOCON_FUNC_1);
   Chip_ADCDAC_SetMuxDAC(NSS_ADCDAC0, ADCDAC_IO_ANA0_0);
   Chip_ADCDAC_SetModeDAC(ADCDAC_IO_ANA0_0, ADCDAC_SINGLE_SHOT);
   Chip_ADCDAC_WriteOutputDAC(NSS_ADCDAC0, 3000);
I got a voltage pulse, then it returns to zero.
If I change the SetModeDAC to ADCDAC_CONTINUOUS, the voltage is held at the appropriate level.
Shouldn't the Output Hold Amplifier keep the output voltage continuous in Single-Shot, or what am I missing?
标记 (1)
4 回复数

2,719 次查看
rcorder
Contributor I

Dries, Thanks for checking on this for me.

Has there been any characterization about the output "hold" amplifier (I used "" because it doesn't hold very long).  Single-Shot mode doesn't seem too useful if 1) it doesn't hold, or 2) its decay isn't characterized.

Rod

0 项奖励
回复

2,719 次查看
driesmoors
NXP Employee
NXP Employee

Hi [email protected],

I could not find any characterization. As you said, single-shot mode just isn't very useful here. Also, decay is dependent on the other connection of the analog line.

Best,
Dries.

0 项奖励
回复

2,719 次查看
driesmoors
NXP Employee
NXP Employee

Hi,

I asked around, and your observations are correct. The DAC functionality is not in a separate HW block, but is provided by the ADC HW block. The NHS3152 IC cannot hold the voltage level for a long duration in single-shot mode. If you need this, you must perform the conversion continually, as you already found out.

Kind regards,
Dries.

0 项奖励
回复

2,719 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

I am sorry, but from my understanding, that is just what single-shot should behave, otherwise what is the difference between single-shot and continuous mode?


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复