NHS3152 ADC conversion - determining conversion equation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NHS3152 ADC conversion - determining conversion equation

1,092 次查看
isaacseeto
Contributor I

Hi, 

I was just wondering if someone could explain how the ADC conversion equations were determined for these posts:

https://community.nxp.com/t5/NFC/NHS3152-ADC-convertion-and-accuracy/m-p/862734/thread-id/4896

https://community.nxp.com/t5/Other-NXP-Products/NHS3152-reading-data-form-NFC/td-p/1585506

I am currently just trying to read voltage to one analog pin. 

标签 (2)
0 项奖励
回复
1 回复

1,031 次查看
patrickgeens
NXP Apps Support
NXP Apps Support

Hello Isaac,

 

The ADC conversion has non-linear behavior at 0V and at the maximum of the input range, therefore it is more accurate to use the Via, min and Via, max values from the datasheet as the voltages corresponding to raw ADC values 0 and 4095. See graph below.

The conversion formula from raw ADC to ADC input voltage (Via) is then:

Via = Via, min + (Via, max - Via, min) * ADCraw / 4095.0

Values outside the Via, min and Via, max cannot be measured: raw value clipped at 0 or 4095.

 

A example measurement showing the behaviour at the top and bottom of the voltage range:

patrickgeens_0-1713786378404.png

 

The Via, min and Via, max values for both ranges, from the NHS3152 datasheet:

patrickgeens_3-1713787733410.png

 

Kind regards,

Patrick

 

0 项奖励
回复