NHS3100 debugging error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NHS3100 debugging error

2,637件の閲覧回数
tillostermann
Contributor II

Hi,

I'm just starting to work with the NHS3100 board, but have issues getting the NHS3100 debugging started in the lpcexpresso IDE. I've worked along the "getting started" guide, but get stuck at connect to emulator.

I have a Win 7 machine connected to a LPC link 2 rev B board which is connected to the NHS3100 demo board. Flashing with flash magic works. Drivers are installed.

Help appreciated!

BR

0 件の賞賛
返信
2 返答(返信)

2,480件の閲覧回数
driesmoors
NXP Employee
NXP Employee

Hi,

Possibly the LPC-Link2 board still contains the debugger firmware from Flash Magic. That one is incompatible with the debugger firmware LPCXpresso uses/expects. Can you power-cycle the board and try again?

Also, be sure to read:

  • <SDK>/docs/UM_NHS31xx_GettingStarted.pdf
  • <SDK>/docs/firmware.html > SW Debug Considerations 

 

Good luck!

0 件の賞賛
返信

2,480件の閲覧回数
tillostermann
Contributor II

Hi,

I've got it working. It really seems like I had the wrong firmware on the LPC-Link board. As I run it in a virtual machine, the usb adapter renames itself and needs to be connected afterwards again.

Thank you for your help!

BR

0 件の賞賛
返信