NHS3100 RTC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NHS3100 RTC

1,698件の閲覧回数
fantasy
NXP Employee
NXP Employee

My customer used NHS3100 internal RTC with 32kHz FRO clock. There's considerable deviation for the RTC.

At room temperature, the deviation is less than 10s per two days;

If placed two boards in the fridge, where the ambient temp is about -10~-20℃, the deviation between the two boards is about 20min per day. While with sw calibration, the deviation could be reduced to several minutes. 

Customer questions are:

1. Do we have the accuracy characteristic of the internal 32kHz FRO clock/ RTC?

2. Do we have ANs or suggestions to improve the RTC accuracy of wide circumstance temp range?

ラベル(1)
0 件の賞賛
返信
1 返信

1,582件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Fantasy,

If you download the NHS3100 SDK(https://www.nxp.com/webapp/Download?colCode=RELEASE-MRA2-NHS3100-11_2&appType=license&Parent_nodeId=... ), you may find the app note on this topic in that package. Please refer to the following for more details.

pastedImage_247.png

Hope that helps,


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信