NFC University Project

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC University Project

1,439件の閲覧回数
davidsagasta97
Contributor I

Hi. I am interested on spent from 300h to 500h on a project regarding NFC and im interested in NXP boards and controllers to do so.

The Project i had in mind was conecting an NFC reader to a simple motor (to resemble a door lock) and that was conected to an online server ( that might be done with an ESP38 and arduino mini ) that allows or denys some cards depending on the online server.

I just want to do a single NFC reader that could be supplied with a battery and that at the same time would improve my knowledge in embbeded systems.

 

Is the OM27462CDK a good kit for my pourpose or are there others fancier?

0 件の賞賛
返信
1 返信

1,384件の閲覧回数
stephanie_m
NXP TechSupport
NXP TechSupport

Hello,

One of the benefits of the PN7462 it's that is one of our best NFC readers,this might be a good option for what you are looking for as this IC does not need an external MCU.

You can check this video that might guide you and help you in the recommendations and development.

NFC application: Access control | NXP 

Hope this helps

Regards,

Estephania

0 件の賞賛
返信