NFC Tag Writer App

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Tag Writer App

4,193 Views
christiannickerson
Contributor I

I'm using the NFC Tag Writer to write ID wristband tags with unique idenitfiers (15-digit text field).  It works fine manually, but I'm having trouble uploading a CSV file so I can write 1000+ tags easily.  Does someone have a sample CSV file that works?  I only need 1 field per line.  This is critical for an event we are having next week. 

 

Message: "No NDEF records found."

 

thank you in advance for your help

 

Christian

Tags (1)
0 Kudos
Reply
2 Replies

4,179 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello @christiannickerson ,

 

Please kindly refer to the link below:
https://tagbase.ksec.co.uk/read-write/tagwriter-android/ , which includes a template CSV file for your reference.

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

4,049 Views
pmeacham3
Contributor I

The template csv file is a dead link.  Please send an updated link or attach the file here.

 

Thanks

0 Kudos
Reply