NFC Tag Emulation & iOS + Android

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Tag Emulation & iOS + Android

10,569 Views
sujit1
Contributor I

Hi, 

Have an application whereby I need a NFC Controller, a user scans the device and is directed to a web-site.

The URI must be programmable and prefer a controller over a frontend. 

Can an Iphone (7 onwards) or Android phone auto scan/read a PN7462 and then be directed to a web-site as per the information in NDEF URI?

And this website could be varied based on some info coming through SPI/I2C or USB etc?

Does there need to be a specific App developed on the phone or will a pop-up be presented where the user can accept and then be directed to the web-site?

- Thanks for your support! 

Tags (3)
0 Kudos
Reply
1 Reply

9,946 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Hope you are doing well. The PN7462 is Full NFC Forum and EMVCo 2.6 compliant

  • Read/Write, Card Emulation & Peer-to-Peer Modes.
  • Full MIFARE family support and ISO/IEC 14443 Type A&B licensed.

 

IOS phones can interact with a reader in card emulation mode, (so the PN7462 is a good choice). So you will be able to use your IOS or Android phone with the reader in card emulation mode.

 

The PN7462 has four different interfaces for host connection: USB, HSUART, I2C and SPI.

 

There is no needed a special App. If the NDEF message is correct, the phone will automatically directed to the web site.

 

Also please check our NTAG 424 family this tags have a feature called SDM  (Secure Dynamic Messaging) this can create an dynamic URL NDEF, please check if this can be solved with that family of tags as well.

 

Best Regards,

Ricardo