NFC TAG'S READER

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NFC TAG'S READER

2,077 次查看
mohamednacer_sa
Contributor I

Hi,I have started my new project which is a NFC tag's reader I choose to work with PN7150 but I dont know which version to use.

Can anyone helps me to select the suitable one 

thank you 

0 项奖励
回复
2 回复数

2,004 次查看
nxf58474
NXP Employee
NXP Employee

Hi [email protected],

 

Hope you are doing well. You can see the versions of the PN7150 in section 6 of the Data Sheet.

 

You can buy the C11006 directly in our page, or if you are interested in the C11002 version, you can buy it to one of our distributors. One important remark, is the IC packing method. (E: TRAY, Y: REEL).

pastedImage_5.png

pastedImage_6.png

The recommendation would be to use the version C11006, as it includes the new features and fixes mentioned in the Data Sheet.

 

Hope this helps.

 

Best Regards,

Ricardo

0 项奖励
回复

1,919 次查看
zhichaotan
Contributor I

hi,if the pn7150 hardware switch to c11006 from c11002, it is there anything need to modify in the Android lower driver? Or can it be replaced directly?

0 项奖励
回复