NFC Product with Card emulation mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC Product with Card emulation mode

Jump to solution
4,128 Views
andy_kim
Contributor IV

Hello,

NTAG I2C Plus is the product for ESL Tag solution.

It has Zero Power Access and Energy Harvesting feature, but it does not have a card emulation mode.

 

Could you tell me which NFC product is fit for ESL Tag which needs card emulation mode with Zero power Access and Energy Harvesting support?

 

Thanks,

Andy 

0 Kudos
Reply
1 Solution
4,104 Views
fangfang
NXP TechSupport
NXP TechSupport
4 Replies
4,119 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Card emulation is the function of reader. TAG itself is a card, which means TAG is a real card, don't need to be emulated.
Hope it help you.
 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 Kudos
Reply
4,114 Views
andy_kim
Contributor IV

Dear fangfang,

 

Thanks for your comment.

 

Let me ask like this.

When customer would like to pay with his phone through ESL Tag of goods,

What NFC Product do you recommend for the ESL Tag solution?

As you mentioned, NFC Tag IC is not proper for the payment via ESL tag.

I wonder if there is a NFC Product that has been applied to ESL tag for that solution.

 

Thanks,

Andy

0 Kudos
Reply
4,105 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

One may refer to the NFC reader as the link.

URL:https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers:NFC-READER.

 

4,099 Views
andy_kim
Contributor IV

Dear fangfang,

 

Thanks for your help.

0 Kudos
Reply