NFC FCC test software

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC FCC test software

2,706件の閲覧回数
donsch
Contributor I

My company has completed a design using the NXP PN7150B0HN and are getting ready for FCC, IC, and CE certifications.  Being new to certification testing does NXP have any test software available that will put the NFC RF into the correct modes for testing?

Thanks

0 件の賞賛
返信
2 返答(返信)

1,650件の閲覧回数
flesky
Contributor II

Hi Team iam searching for such a Programm to run on PN7462?

for certification we need this operating modes:

RF on CW

RF on  send PRBS

RF off

 

THank you very much

0 件の賞賛
返信

2,563件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hello Don,

The Linux FactoryTestApp is specifically designed for this.
It is depicted in the http://www.nxp.com/documents/application_note/AN11697.pdf, and the related github repository address is here: https://github.com/NXP/nfc-linux_NfcFactoryTestApp.

Hope that helps,

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信