NFC FCC test software

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NFC FCC test software

2,807 Views
donsch
Contributor I

My company has completed a design using the NXP PN7150B0HN and are getting ready for FCC, IC, and CE certifications.  Being new to certification testing does NXP have any test software available that will put the NFC RF into the correct modes for testing?

Thanks

0 Kudos
Reply
2 Replies

1,751 Views
flesky
Contributor II

Hi Team iam searching for such a Programm to run on PN7462?

for certification we need this operating modes:

RF on CW

RF on  send PRBS

RF off

 

THank you very much

0 Kudos
Reply

2,664 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hello Don,

The Linux FactoryTestApp is specifically designed for this.
It is depicted in the http://www.nxp.com/documents/application_note/AN11697.pdf, and the related github repository address is here: https://github.com/NXP/nfc-linux_NfcFactoryTestApp.

Hope that helps,

Have a great day,
Kan

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply