NFC Cockpit issue under Windows 10

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Cockpit issue under Windows 10

ソリューションへジャンプ
4,461件の閲覧回数
jean-pierrefort
Contributor II

Hi,

I'am trying to work with the PNEV7462B eval board and the NFC Cockpit tool (v1.3.0.0) under Windows 10.

I have successfully updated the board (firmware and eeprom) through the mass storage 'channel'.

After reboot, a new USB virtual serial port appeared (COM11) but Cockpit doesn't see it. The port selector combo is empty.

I also reinstalled the VCOM driver (forcing Windows 10 to install unsigned drivers) but the result is the same.

Is there a known issue around this?

Thanks in advance for your help.

-- 

Jean-Pierre

ラベル(1)
0 件の賞賛
返信
1 解決策
3,803件の閲覧回数
jean-pierrefort
Contributor II

Finally it works after reinstalling the VCOM driver using another method:

peripherals->update driver->choose driver in list->select PN7462AU VCOM Port.

The device name now appears as PN7462AU VCOM (COM11)

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,803件の閲覧回数
jean-pierrefort
Contributor II

After a new positive test done under Windows XP running in a VM on the same computer, the issue met under W10 is clearly related to the installation of the PN7462 VCOM driver.

To be continued...

0 件の賞賛
返信
3,804件の閲覧回数
jean-pierrefort
Contributor II

Finally it works after reinstalling the VCOM driver using another method:

peripherals->update driver->choose driver in list->select PN7462AU VCOM Port.

The device name now appears as PN7462AU VCOM (COM11)

0 件の賞賛
返信