NFC Cockpit HAL, IO_TIMEOUT

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NFC Cockpit HAL, IO_TIMEOUT

4,540件の閲覧回数
HP009
Contributor I

Testing CLRC663 plus development board with NTAG212

1. Load protocol (106kBd/s) - no error

2. RF field On - no error

3. Activate layer 3 - ERROR:RFProtocolTypeAService:RequestA Failed HAL,IO_TIMEOUT

 

How to resolve this?

0 件の賞賛
返信
3 返答(返信)

4,525件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hello,

 Before activating Layer 3, please approach the tag.

Hope  it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信

3,654件の閲覧回数
nitinGangurde2001
Contributor I

The solution which you have given is not working for me. Can you give me other solution for it.

 

0 件の賞賛
返信

4,519件の閲覧回数
HP009
Contributor I

Tag was already placed on the antenna of the development board. Antenna of the tag is very small 3.0x3.0mm.If output power density of the larger antenna is lower, since this tag's antenna is small induced power might be insufficient right? Could this be the problem? Larger tags(which came with the development kit) works. Is there a way to increase the power ? or If i swap the larger antenna for the smaller one will power density increase?

0 件の賞賛
返信