NFC Antenna Crossing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
3,664件の閲覧回数
nike9307
Contributor II

Hi all,
I was looking at some NXP dev kits and noticed something curious.
Some kits (like on the PN5180 and the CLRC663) have a antenna that is crossed on the "far" end of the antenna. As far as possible compared to the input signals on the connectors. 

Far_end.jpg

The PN5190 dev kit has the antenna crossing on the near end. 

Near_end.jpg

Does it have any effect on the field. If yes, what are the ups and downs of each design?

0 件の賞賛
返信
1 解決策
3,655件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nike9307 ,

 

Indeed the difference is between even or odd number of turns.


The target is to make the coil as symmetrical as possible. so the PCB layout style for PN5180/CLRC663 kev kit is recommended , but in fact the overall impact is minor.

Please be aware NOT to copy the copper tiles inside the antenna area: those copper tiles are made only to “emulate” a bad antenna, and must not be copied!

We also provide a ready to use NFC antenna dev kit, you may refer to https://www.nxp.com/part/OM29263ADK#/ for details.

 

Regarding a good number of turns, please refer to our NFC antenna tool - https://community.nxp.com/t5/NFC/bd-p/nfc .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,656件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nike9307 ,

 

Indeed the difference is between even or odd number of turns.


The target is to make the coil as symmetrical as possible. so the PCB layout style for PN5180/CLRC663 kev kit is recommended , but in fact the overall impact is minor.

Please be aware NOT to copy the copper tiles inside the antenna area: those copper tiles are made only to “emulate” a bad antenna, and must not be copied!

We also provide a ready to use NFC antenna dev kit, you may refer to https://www.nxp.com/part/OM29263ADK#/ for details.

 

Regarding a good number of turns, please refer to our NFC antenna tool - https://community.nxp.com/t5/NFC/bd-p/nfc .

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
3,652件の閲覧回数
nike9307
Contributor II

Hi @Kan_Li 

Thank you for the quick reply. It was very helpful.

I'm aware about the tiles and their function. 

I've always tended to use the standalone exe NFC Antenna Tool you used to provide. Is the online version better than the standalone one? The only difference i see is the addition of the dielectric field. 

0 件の賞賛
返信
3,635件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @nike9307 ,

 

Yes, the online version is the latest.

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信