NDEF writing error through I2C interface

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

NDEF writing error through I2C interface

2,084件の閲覧回数
andy_kim
Contributor IV

Hello,

We have a problem of writing NDEF message to NTAG I2C through I2C Interface from BLE IC.

When we write NDEF message to EEPROM through NFC Interface using NTAG I2C Demo application, The writing is OK and then if we tap NFC phone to ESL tag, it works well showing the internet website as we wrote to NDEF message.

However, After we wrote NDEF message to EEPROM through I2C interface. When we tap NFC phone with NTAG I2C Demo app to ESL Tag, It shows "TAG unknown" error message on the screen.

 

What we found out is that the content of 03h(CC) between them are different.

In case of writing NDEF message through NFC Interface,

The content of 03h(CC) has a specific number.

When it comes to writing NDEF message through I2C interface,

The content of 03h(CC) are all zero( 00:00:00:00)

Let me attach the picture of the Memory content for your refer.

 

Did we miss something when we write NDEF message through I2C interface?

Please let us know how to fix the issue. 

 

Thanks you,

Andy

0 件の賞賛
返信
1 返信

2,075件の閲覧回数
Ricardo_Zamora
NXP TechSupport
NXP TechSupport

Hi Andy,

 

Hope you are doing well. Could you make a full scan with NFC TagInfo by NXP? Please share the memory content of your two scenarios: NFC and I2C writing.

Also, do you have a logical analyzer to see if your BLE IC is accessing correctly to the tag memory?

 

Best Regards,

Ricardo

0 件の賞賛
返信