NCx3321 communication problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

NCx3321 communication problem

1,595 次查看
Christiane
Contributor I

Hello,

I have a S32K118 evaluation board and a NCx3321 S32K Addon board3.
I try to communicate through SPI but the NCx3321 does not answer.

Application note AN790311 shows some examples for the communiction. After sending a command frame there should be a interrupt to signal that date can be read.
But the IRQ line never changes to high level. And the chip never responses any data.

The IRQ line is connected with an input and configured to generate an interrupt on rising edge. This works when i manually change the level at this input.

How can I communicate with this chip?

Do I need further presets?

Thanks in advance

Christiane Eibeck

0 项奖励
回复
2 回复数

1,542 次查看
stephanie_m
NXP TechSupport
NXP TechSupport

Hello, 

 

As you might know, there are some of the documents and libraries which are under NDA (Non-Disclosure Agreement)

Could you please help us contact the person that helped you getting the device. The NCx3321 information is under NDA . 

 

Regards

0 项奖励
回复

1,583 次查看
Christiane
Contributor I

I use the NXP Eval-board and the NXP NFC Addon-board. The Addon-board is made to plug onto the S32K Eval-Board. So there should be no problems with wiring or level shifters. The SPI settings (CPOL/CPHA) ar set to the demanded values.

The SPI communication generally works with other devices. And of course I use a logic analyzer to check the communication.

0 项奖励
回复