Mifare&NFC licence

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mifare&NFC licence

4,855 Views
adamjansky
Contributor I

Hi,

if we use NXP product (like PN5120) does it mean that we fulfil the licence conditions necessary for Mifare (classic, DesFire,..) plus NFC A, B? To get support regarding DesFire we need to sign NDA?

We are developing readers for access control systems, so we plan to use mifare and or NFC for access. I found good document covering NFC licence topic, but not too much regarding Mifare.

thank you,

best regards

Adam.

Labels (2)
Tags (2)
0 Kudos
Reply
3 Replies

4,404 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Adam Jansky,

For the ISO/IEC 14443A and ISO/IEC 14443B licensing information, see the next page:

ISO/IEC 14443A Licensing Information|NXP 

Regarding MIFARE, please visit the next pages about certification and branding:

Certification | MIFARE

Trademark and Branding Information | MIFARE 

The MIFARE DESFire documentation is indeed protected under NDA. You need to contact your local authorized distributor:

Distributor Network|NXP 

Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

4,404 Views
michaelbiggs
Contributor I

Your link for ISO/IEC 14443A and ISO/IEC 14443B licensing information doesn't work.

0 Kudos
Reply

4,404 Views
adamjansky
Contributor I

Hi Jorge,

Please see my comments below.

Do you cover Czech Republic (sales representative, AFAE,..)?

Best regards

Adam.

0 Kudos
Reply