Mifare&NFC licence

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Mifare&NFC licence

4,858件の閲覧回数
adamjansky
Contributor I

Hi,

if we use NXP product (like PN5120) does it mean that we fulfil the licence conditions necessary for Mifare (classic, DesFire,..) plus NFC A, B? To get support regarding DesFire we need to sign NDA?

We are developing readers for access control systems, so we plan to use mifare and or NFC for access. I found good document covering NFC licence topic, but not too much regarding Mifare.

thank you,

best regards

Adam.

ラベル(2)
タグ(2)
0 件の賞賛
返信
3 返答(返信)

4,407件の閲覧回数
Jorge_Gonzalez
NXP Employee
NXP Employee

Hello Adam Jansky,

For the ISO/IEC 14443A and ISO/IEC 14443B licensing information, see the next page:

ISO/IEC 14443A Licensing Information|NXP 

Regarding MIFARE, please visit the next pages about certification and branding:

Certification | MIFARE

Trademark and Branding Information | MIFARE 

The MIFARE DESFire documentation is indeed protected under NDA. You need to contact your local authorized distributor:

Distributor Network|NXP 

Best Regards!,
Jorge Gonzalez

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,407件の閲覧回数
michaelbiggs
Contributor I

Your link for ISO/IEC 14443A and ISO/IEC 14443B licensing information doesn't work.

0 件の賞賛
返信

4,407件の閲覧回数
adamjansky
Contributor I

Hi Jorge,

Please see my comments below.

Do you cover Czech Republic (sales representative, AFAE,..)?

Best regards

Adam.

0 件の賞賛
返信