Mifare DesFire Authentication

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Mifare DesFire Authentication

4,360 Views
henrichgregac
Contributor I

Hello

I would like to ask about Mifare Desfire Ev1
I have one problem with authentication 3-pass mutual.(with default MasterKey 16 bytes 0x00)
In last step when compare RndA and RndA' is not equal.But I dont know why.
Because step befor Card send Status = 0x00(is OK..Authenticate).

I created application in C# and I use SL032 reader interfae.
And this is my communication.(S-send from PC)(R-received from Card)
S:0A 00 -> R:AF DE D4 E1 04 62 13 C5 B2
S:DB 47 CC D2 10 DA 8A 43 33 2B 67 E4 DD 8D C7 95  R:00 7C B5 65 E3 8B 65 BA 74 (this is last frame from CARD first byte is Status)

And I use same implementation TripleDes(.net framework implementation TripleDESCryptoServiceProvider with CipherMode.CBC,PaddingMode.Zeros)
in first step when I decrypt(IV= 8bytes 0x00) RndB' from card it is OK.
in second step when I encrypt(IV=EncRndB[8bytes received in first step]) RndA and RndB it is OK because response from card is status:0x00.

Can you help me why in last step when I decrypt(IV = second half SendData in second Step[enc RndB']) data from card is something  wrong because is not same like RndA(I generated in first step)?


Thank you for answer.

Best Regards

0 Kudos
Reply
1 Reply

3,360 Views
soledad
NXP Employee
NXP Employee

Hello Henrich,

For the moment, this is under NDA. Therefore it may be recommended to apply to local NXP representative or FAE who will be able to assist.

If you do not know how to find the local sales office (or FAE), please call our Technical Information Center. Sales and Support|NXP

Have a great day,
Sol

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply