Maximum range with CLRC663 plus up-to 1m

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Maximum range with CLRC663 plus up-to 1m

1,562 Views
lakshminarayana
Contributor II

May I know what maximum range can be achieved with CLRC663 plus?

 

I read that it can up to 1.5meters but in the forum, it's mentioned as around 30cm.

With CLRC663 plus, ICODE SLIX 2 Tag can we achieve a range of 1m?

Is the development board CLRC663 plus tested with ICODE SLIX2? If yes what's the maximum range.

Could you please guide us to some of the manufacturers of ICODE SLIX2 tags?

0 Kudos
Reply
2 Replies

1,548 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

For more information please refer to the  thread https://community.nxp.com/t5/Other-NXP-Products/CLRC663-Long-range-reader-up-to-50cm/td-p/1204941.

And you can test the board performance of CLRC663 Plus as the link.

URL:https://www.nxp.com/products/rfid-nfc/nfc-hf/nfc-readers/clrc663-iplus-i-nfc-frontend-development-ki....

Hope it help you. Have a nice day.

 

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

 

0 Kudos
Reply

1,536 Views
lakshminarayana
Contributor II

Thank you.

I've reviewed those thread earlier but which do not get a clear picture about the range with the SLIX 2 tag.

So asking again Is the EVK tested with SLIX2 Tag? If so what's the max range possible?

0 Kudos
Reply