MIFARE supported bitrates

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIFARE supported bitrates

跳至解决方案
3,731 次查看
piergiuseppe_tu
Contributor II

https://www.mifare.net/wp-content/uploads/2015/02/MIFARE-Z-Card-2017.pdf  reports that Ultralight and Classic support only 106kbps communication speed, whereas, once queried by RATS they both report a TA(1)=0x77 in their ATS response (complete response: 0x06 0x75 0x77 0x81 0x02 0x80).

I'd like to know who's telling the truth and who's not.

Thank you in advance,

P.

标记 (2)
1 解答
3,636 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi Piergiuseppe Tundo, 

Hope you are doing great, please follow the documentation in our webpage and in Mifare.net as you may know this two tags are T2T which means the speed is 106kbps.  you are saying the cards answer with a RATS, well this is not possible  directly form the cards, since this cards are ISO 14443-3 they answer to a REQA command with ATQA, this will activate the card in ISO 14443-3 to activate a card in layer 4 of this iso ( which is the layer for smartcards like DESFire or Plus)  you send a RATS and the card answers with an ATS. I assume you might be using a PC/SC reader device that  usually work on layer 4, and  when a type 3 tag is detected a pseudo ATS is generated to comply with the reader communication. 

please follow the NXP documentation available

BR

Jonathan

在原帖中查看解决方案

2 回复数
3,637 次查看
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Hi Piergiuseppe Tundo, 

Hope you are doing great, please follow the documentation in our webpage and in Mifare.net as you may know this two tags are T2T which means the speed is 106kbps.  you are saying the cards answer with a RATS, well this is not possible  directly form the cards, since this cards are ISO 14443-3 they answer to a REQA command with ATQA, this will activate the card in ISO 14443-3 to activate a card in layer 4 of this iso ( which is the layer for smartcards like DESFire or Plus)  you send a RATS and the card answers with an ATS. I assume you might be using a PC/SC reader device that  usually work on layer 4, and  when a type 3 tag is detected a pseudo ATS is generated to comply with the reader communication. 

please follow the NXP documentation available

BR

Jonathan

3,636 次查看
piergiuseppe_tu
Contributor II

Hi Jonathan, thank you very much for your prompt reply.

I'm using PN7462 and NFC Reader Library but I forgot to reset ATS buffer before each discovery loop, so I was actually decoding stale ATS from previously detected T4T cards.

Thank you again.

P.