MIFARE classic and plus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MIFARE classic and plus

3,078 次查看
giulio_favre
Contributor I

Hello community,

I have to design a system able to read MIFARE classic 4K and MIFARE Plus 2K, I can't chose the microcontroller and the one I have to deal with is an STM32L4. I have non experience with NFC and smart cards in general so I'm not sure what would be most suitable device and perhaps the simplest to be ported on STM32. 

Any suggestion will be appreciated.

Thanks

Jule

标记 (1)
0 项奖励
回复
2 回复数

2,858 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

You may be interested to take a look to the following front end for MIFARE and NTAG: MFRC630 plus | NXP 

For the software, please refer to the Tools & Software section in which you will find the NFC Reader Library which you can take as a reference: MFRC630 plus | NXP 

BR,

Ivan.

0 项奖励
回复

2,858 次查看
giulio_favre
Contributor I

Thank you very much Ivan, I had a look to the library you are referring to. It looks very promising but, as far as I understand, MIFARE Plus is not included, am I wrong? shall I look somewere else?

thanks

Jule

0 项奖励
回复