MIFARE PLUS X: how to handle AES encryption in flutter

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIFARE PLUS X: how to handle AES encryption in flutter

跳至解决方案
1,409 次查看
Matthew1971
Contributor II

Hello,

I bought a few Mifare Plus X cards for testing using flutter.
To do AES encryption and decryption for data writing and reading on the card, do i use flutter or there is some inbuilt feature in Mifare Plus X that i can use ? If yes, how to use those feature in flutter ? Any URL reference ?

Thank you

Matthew1971 

标记 (1)
0 项奖励
回复
1 解答
1,392 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Matthew1971 

Since NXP does not have example based on Flutter, but we recommend you to use Taplinx to develope MIFARE PLUS products. Maybe you can refer to the below SDK examples:

TapLinx SDK for MIFARE, NTAG, ICODE and UCODE | NXP Semiconductors

 

KellyLi_0-1737527746979.png

 

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,393 次查看
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Matthew1971 

Since NXP does not have example based on Flutter, but we recommend you to use Taplinx to develope MIFARE PLUS products. Maybe you can refer to the below SDK examples:

TapLinx SDK for MIFARE, NTAG, ICODE and UCODE | NXP Semiconductors

 

KellyLi_0-1737527746979.png

 

 

0 项奖励
回复
1,376 次查看
Matthew1971
Contributor II

@KaiLi 

Thank you for the helpful suggestion and reference, i am now going through the user guide.

Questions
1. Do I need to pay for the TapLinx SDK ? Is it free ?
2. If i purpose the Mifare Plus card from Shopee, is this card compatible with the TapLinx SDK ?
Shopee order reference: https://shopee.com.my/13.56MHZ-(IC)-MIFARE-CUID-GEN2-GEN1-Mifare-Plus-S-2K-RFID-1K-S50-F08-FM1108-DU...

Pls advise

Thank you
Matthew

0 项奖励
回复