MFRC630 no response from LPCD Interrupt mode

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MFRC630 no response from LPCD Interrupt mode

1,782件の閲覧回数
santosh2
Contributor I

Hello All,

We have designed Low Power RFID based device where we are using MFRC630 Plus reader chip,with Mifare 1K classic card.

After reading version register of the RFID Chip we are understand this is MFRC63002 chip as per data sheet, also we have read Mifare 1K classic card.


We wanted configure LPCD(Low Power Card Detection) Interrupt for which we made respective configuration but i am not able to get LPCD Interrupt.


However  if we configure any of TIMER interrupts(TIMER0 TO TIMER4) we are able to get interrupts.


we are not able to  understand where we are going  wrong please find below code for LPCD interrupt Configuration.

 

 

SoftReset(); //Soft reset the RFID chip
MFRC630CmdIdle();
MFRC630FlushFifo();
// Configure Radio Protocol
MFRC630AN1102recommendedregisters(MFRC630PROTOISO14443A106MILLERMANCHESTER);
MFRC630WriteReg(MFRC630_REG_DRVMOD, 0x8E);
MFRC630WriteReg(MFRC630_REG_TXAMP, 0x12);
MFRC630WriteReg(MFRC630_REG_DRVCON, 0x39);
MFRC630WriteReg(MFRC630_REG_TXL, 0x06);
uint8_t instruction;
// ready the request.
uint8_t send_req[] = {instruction};

MFRC630WriteReg(0x06, 0x7F); // clear interrupts
MFRC630WriteReg(0x07, 0x7F);

MFRC630WriteReg(0x08,0x80);
MFRC630WriteReg(0x09,0xE0); //only trigger on LPCD for irq1

MFRC630WriteReg(0x24, 0x00); // Write min. T4 reload value Hi
MFRC630WriteReg(0x25, 0x05); // Write min. T4 reload value Lo
MFRC630WriteReg(0x23,0xDC); // Config T4 for AutoLPCD&AutoRestart.Set AutoTrimm bit.Start T4.
while(!(MFRC630ReadReg( 0x23) & 0x80))
{
MFRC630WriteReg( 0x23 , 0xDC);
}
MFRC630WriteReg(0x43, 0x40);
while(!(MFRC630ReadReg(0x00) & 0x80))
{
MFRC630WriteReg(0x00, 0x41);
}

 

 


I would request if possible can any one please help us with LPCD interrupt configuration at your earliest.

Please let me know if there any mistakes or modification which we are missing for LPCD configuration.

Regards
Santosh P

タグ(1)
0 件の賞賛
返信
1 返信

1,767件の閲覧回数
fangfang
NXP TechSupport
NXP TechSupport

Hi @santosh2 ,

Actually there is a LPCD demo "NfcrdlibTst12_Rc663Lpcd " available in the latest NFC reader library, and we also provide the following app note on LPCD topic, Please kindly refer to the following for details.
https://www.nxp.com/docs/en/application-note/AN11783.pdf.

And you may refer to the information for your application.

 

 

Have a nice day.

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------

0 件の賞賛
返信