LPC Link 2 fails to program PN7462 by reporting error "can not halt processor".

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC Link 2 fails to program PN7462 by reporting error "can not halt processor".

1,805 Views
mayank_sharma1
Contributor III

LPC Link 2 fails to program PN7462 by reporting error can not halt processor.

The only way to recover the chip is to activate USB bootloader. In our design we are not using USB and I need support to fix this issue. 

How come NXP designing MCU that can not be programmed by debugger/SWD?

I never had such a bad experience in past with any other vendor. 

Following is the log from LPC Link. 

MCUXpresso RedlinkMulti Driver v10.0 (Jun 22 2017 23:31:55 - crt_emu_cm_redlink build 272)
Reconnected to existing redlink server (PID 4294967295)
Connecting to probe 1 core 0 (server PID unknown) gave 'OK'
============= SCRIPT: PN7xxxxx_Connect.scp =============
DpID = 0BB11477
APID = 0x04770021
============= END SCRIPT ===============================
Probe Firmware: LPC-LINK2 CMSIS-DAP V5.182 (NXP Semiconductors)
Serial Number: I3F2E2KT
VID:PID: 1FC9:0090
USB Path: \\?\hid#vid_1fc9&pid_0090&mi_00#7&c19723b&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Cannot halt processor
Cannot halt processor
number of h/w breakpoints = 0
number of flash patches = 0
number of h/w watchpoints = 0
Probe(0): Connected&Reset. DpID: 0BB11477. CpuID: 410CC200. Info: <None>
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Cannot halt processor
Failed on chip setup: Ep(04). Cannot halt processor.

0 Kudos
Reply
2 Replies

1,554 Views
ivan_mihajlov
Contributor I

Hello,

I have the same problem. If you figured out the solution, please let me know :smileyhappy:

Regards,
Ivan

0 Kudos
Reply

1,554 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Have you tried to Flash an unmodified example of the Nfc Reader Library?

Regards,

Ivan.

0 Kudos
Reply