Interfacing NTAG I2C with Freedom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing NTAG I2C with Freedom board

1,594 Views
bheemarao
Contributor II

Hi,

I am looking to interface NTAG I2C plus Antenna board (NT3H2111/2211) that comes along with OM5569/NT322E with FRDM-K64 freedom board.

Is there any interfacing example code available in KDS or processor expert interfacing to any freedom board with this NTAG board.

Regards

Bheema Rao

0 Kudos
Reply
2 Replies

1,083 Views
Jorge_Gonzalez
NXP Employee
NXP Employee

Hi Bheema Rao,

If you are still looking for this you might want to look at the next document:

https://community.nxp.com/docs/DOC-333498 

Regards!

Jorge Gonzalez

0 Kudos
Reply

1,083 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Bheema Rao,

There is LPC based project for your requirement, but so far no FRDM-K64 based project yet, you might have to port the code. Please kindly refer to http://www.nxp.com/documents/software/SW3647.zip for details.


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply