Increase HTRC110 Tag reading

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Increase HTRC110 Tag reading

1,538件の閲覧回数
Felix0209
Contributor II

I have successfully read HITAG S tags and read pages and blocks but it only works when the tag is on top of the coil and not at a distance > 1cm. I can see the tag affects the field at a greater distance but when I look at Dout on the HTRC110 it hasnt demodulated it. I am pretty sure the electrical side is correct as i copied a product that works. is there something that I need to tune in the config page that might help

 

product - https://docs.rs-online.com/73f6/0900766b81641265.pdf

0 件の賞賛
返信
3 返答(返信)

1,510件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

 

Hello, my name is Fabian, I've been assigned to support your case.

Thank you for your interest in our products

My apologies for the delay answering back.

I cannot assure you is the antenna design of the Reader is the optimal since the design was based on a different device. For a successful antenna design and tunning, I have to recommend to please take a look at our HTRC110 documentation:

https://www.nxp.com/docs/en/application-note/AN98080.pdf

I hope this information may have been useful.

Best Regards,
Fabian
0 件の賞賛
返信

1,467件の閲覧回数
Felix0209
Contributor II

I have gone throught the application notes and double checked my circuit is right and it is. I even tried slightly changing some of the resistor values but nothing changed. I can see on a scope the tag is sending data at a distance of about 5cm above and is visible at Rx but then when I scope Dout nothing is demodulated

0 件の賞賛
返信

1,454件の閲覧回数
Fabian_R
NXP TechSupport
NXP TechSupport

Hello sir, I understand.

Still, I will have to ask you to check the antenna Tunning using a Vector Analyzer. Unfortunately we don't have a specific document to perform this procedure in the HTRC, please take a look at our NFC devices. The procedure should be very similar. Please keep in mind that you will need to sweep the frequency around 125kHz.

Please take a look at the following documents: https://www.nxp.com/docs/en/application-note/AN11019.pdf

https://www.nxp.com/docs/en/application-note/AN12810.pdf

 

We are assuming you don't have any power-related issues since reading tags is successful but, it is worth to also check this for discarding a possible issue.

Best Regards,
Fabian
0 件の賞賛
返信