ISO15693 Write Command Response Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ISO15693 Write Command Response Issue

4,761 Views
amolborase
Contributor II

Dear All, 

I have an issue regarding ISO 15693 Write Command. Using Address Flag (0x22) command works fine and also getting success response, but as I am sending frame with Option flag with tag UID (0x62) data get written into tag memory successfully but response I am getting is not success(instead of 0x0000  it gives 0x4f01). Here is  our customised code for Write Single Block :

uint8_t TxBuflength=0;

phhalRf_RxParams_t sRxParams;

uint16_t Status=0xFFFF;

Status = phhalRf_FieldOn();


Status = phhalRf_LoadProtocol_Initiator(E_PHHAL_RF_LP_I_TX_15693_100, E_PHHAL_RF_LP_I_RX_15693_26);
PH_RETURN_ON_FAILURE(Status)

phhalRf_SetConfig(PHHAL_RF_CONFIG_TXWAIT_US, 1200);
phhalRf_SetConfig(PHHAL_RF_CONFIG_RXWAIT_US, 10);
phhalRf_PCD_SetExchgFdt(20000);

if((Flag & ISO15K_ADDRESS_FLAG)==ISO15K_ADDRESS_FLAG) // Check Valid Flag 0x02
{
      phhalRf_PCD_SetExchgFdt(20000);
      Flag |=ISO15K_DATA_RATE_FLAG;
      TxBuffer[TxBuflength++] = Flag;
      TxBuffer[TxBuflength++] = Cmd;
      memcpy(&TxBuffer[TxBuflength],UID,8);
      TxBuflength+=8;

}
else
{
      Flag |=ISO15K_DATA_RATE_FLAG;
      TxBuffer[TxBuflength++] = Flag;
      TxBuffer[TxBuflength++] = Cmd;
}

if((Flag & ISO15K_OPTION_FLAG)==ISO15K_OPTION_FLAG)
{
   Status = phhalRf_PCD_Exchg_TxOnlyEOF(RxBuffer,&sRxParams);
   __NOP();
}

TxBuffer[TxBuflength++] = BlockAddress;

memcpy(&TxBuffer[TxBuflength],(uint8_t *)BlockData,4);

TxBuflength +=4;

Status = phhalRf_PCD_Exchg(TxBuffer,RxBuffer,TxBuflength,&sRxParams); // Exchange function

return Status;

Is anything wrong or missing in above code? Please guide us for the same 

Thanks in Advance

regards,

Amol 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

4,550 Views
Jonathan_Iglesias
NXP TechSupport
NXP TechSupport

Dear Amol Borase,

what ISO 15693 tag are you using and what reader as well ? 

my recommendation would be that you base your code in our NFC reader library first in order to avoid any issue, there is an example available in the NFC reader library  for ISO 15693. 

NFC Reader Library | NXP 

please let me know which products from NXP are you using and whether you are using our library as a base.

Have a great day !
BR

Jonathan

0 Kudos
Reply

4,550 Views
amolborase
Contributor II

Hii Jonathan,

We are using PN7462 Development Board.To develop code for ISO 15693 protocol command using basic internal  library functions as you can see in above given code. All other commands developed like this is working fine with no issue but in case of write with option flag I made configurations  according to NFC library functions example too . Can you please check is there any mistake  we are doing while configuration related to  option flag. Please suggest any changes in configuration in above mention code. 

0 Kudos
Reply