ICODE SLIX2 SL2S2602

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ICODE SLIX2 SL2S2602

3,039件の閲覧回数
pkumar
Contributor I

Hello everyone, I am trying to use SLIX2 tag with PN7120 controller in android and trying to utilize API's of settings password for few blocks for read/write access management and few blocks for EAS/AFI password. To make these working, getRandomNumber command has to work before i write & set password by XORing. 

Here is what I am getting after initial reading of TAG type, checking & parsing system info and finally close the connection. Connect again for further programming the Tag, but after few seconds of connect, TAG was lost :

ID: =: rawCmd: cmd=0x90 F4 D6 00 08 01 04 E0
D/isX  =: false
D/isX2  =: true
D/ICode: Iso15693Tag: connect
D/ICode: Iso15693Tag: getSystemInfo
I/ICode: getCardInfo flags: 32
D/ICode: rawCmd PARAMETERS: nfcVCmd :43 flags: 32 params: [00] 90 F4 D6 00 08 01 04 E0 |.|.|.|.|.|.|.|.|
D/ICode: Inventory in rawCmd : true
D/ICode: addressed in rawCmd : false
D/ICode: cmd in rawCmd : [00] 00 00 00 00 00 00 00 00 |.|.|.|.|.|.|.|.|
                                            [08] 00 00 |. |. |
D/ICode: rawCmd: params.length=0x8
D/ICode: rawCmd: cmd=0x20 2B 90 F4 D6 00 08 01 04 E0
D/ICode: rawCmd: rsp=0x00 0F 90 F4 D6 00 08 01 04 E0 00 00 4F 03 01
D/ICode: SystemInfo: [00] 0F 90 F4 D6 00 08 01 04 |.|.|.|.|.|.|.|.|
                                    [08] E0 00 00 4F 03 01 |. |. |. |O |. |. |
D/ICode: Iso15693Tag: parseSystemInfo
D/ICode: .parseSystemInfo mSysInfo: 0x0F 90 F4 D6 00 08 01 04 E0 00 00 4F 03 01
D/ICode: mSysInfo[0]: 0x0F
D/ICode: Iso15693Tag: checkReadSupport
D/ICode: Iso15693Tag: mUid=0x90 F4 D6 00 08 01 04 E0
D/ICode: Iso15693Tag: mDsfid=0x00
D/ICode: Iso15693Tag: numblocks=80
D/ICode: Iso15693Tag: blocksize=4
D/ICode: Iso15693Tag: mDsfidSupported=true
D/ICode: Iso15693Tag: mAfiSupported =true
D/ICode: Iso15693Tag: mIcRef =1
===============ICodeTag connection close =============
===============ICodeTag connect=======================
D/ICode: rawCmd PARAMETERS: nfcVCmd :-78 flags: 32 params:
D/ICode: Inventory in rawCmd : true
D/ICode: addressed in rawCmd : false
D/ICode: cmd in rawCmd : [00] 00 00 |. |. |
D/ICode: rawCmd: params.length=0x0
D/ICode: rawCmd: cmd=0x20 B2
W/System.err: android.nfc.TagLostException: Tag was lost.
W/System.err: at android.nfc.TransceiveResult.getResponseOrThrow(TransceiveResult.java:48)
W/System.err: at android.nfc.tech.BasicTagTechnology.transceive(BasicTagTechnology.java:151)
W/System.err: at android.nfc.tech.NfcV.transceive(NfcV.java:115)
W/System.err: at com.potrero.acmslix2.ICode.transceive(ICode.kt:382)
W/System.err: at com.potrero.acmslix2.ICode.rawCmd(ICode.kt:446)
W/System.err: at com.potrero.acmslix2.ICodeCommon.getRandomNumber(ICodeCommon.kt:167)
W/System.err: at com.potrero.acmslix2.MainActivity.programTag(MainActivity.kt:256)
W/System.err: at com.potrero.acmslix2.MainActivity.filterIntent(MainActivity.kt:173)
W/System.err: at com.potrero.acmslix2.MainActivity.onNewIntent(MainActivity.kt:415)
W/System.err: at android.app.Instrumentation.callActivityOnNewIntent(Instrumentation.java:1224)
W/System.err: at android.app.Instrumentation.callActivityOnNewIntent(Instrumentation.java:1236)
W/System.err: at android.app.ActivityThread.deliverNewIntents(ActivityThread.java:2803)
W/System.err: at android.app.ActivityThread.performNewIntents(ActivityThread.java:2818)
W/System.err: at android.app.ActivityThread.handleNewIntent(ActivityThread.java:2834)
W/System.err: at android.app.ActivityThread.-wrap15(ActivityThread.java)
W/System.err: at android.app.ActivityThread$H.handleMessage(ActivityThread.java:1557)
W/System.err: at android.os.Handler.dispatchMessage(Handler.java:102)
W/System.err: at android.os.Looper.loop(Looper.java:154)
W/System.err: at android.app.ActivityThread.main(ActivityThread.java:6121)
W/System.err: at java.lang.reflect.Method.invoke(Native Method)
W/System.err: at com.android.internal.os.ZygoteInit$MethodAndArgsCaller.run(ZygoteInit.java:889)
W/System.err: at com.android.internal.os.ZygoteInit.main(ZygoteInit.java:779)

Code :

mTag = tag
mNfcV = NfcV.get(tag)
if (mNfcV == null) {
    return
}
// read UID
mUid = tag.id
// read DFSID if programmed
mDsfid = mNfcV.dsfId

try {
    Log.d(TAG, "Iso15693Tag: connect")
    connect()

    Log.d(TAG, "Iso15693Tag: getSystemInfo")
    val systeminfo = getCardInfoHelper(NFCV_FLAG_ADDRESS)
    Log.d(TAG, "SystemInfo: "+Utils.hexDump(systeminfo))

    Log.d(TAG, "Iso15693Tag: parseSystemInfo")
    parseSystemInfo(systeminfo)


    // If getSystemInfo is not supported, get the blocksize and number
    // of block through read commands
    Log.d(TAG, "Iso15693Tag: checkReadSupport")
    checkReadSupport()

} catch (e: IOException) {
    Log.d(TAG, "Iso15693Tag: Error, no response")
}

try {
    close()
} catch (e: IOException) {
    e.printStackTrace()
}

Log.d(TAG, Utils.dumpHex(mUid, "Iso15693Tag: mUid=0x", " "))
Log.d(TAG, Utils.dumpHex(mDsfid, "Iso15693Tag: mDsfid=0x"))
Log.d(TAG, "Iso15693Tag: numblocks=$mNumBlocks")
Log.d(TAG, "Iso15693Tag: blocksize=$mBlockSize")
Log.d(TAG, "Iso15693Tag: mDsfidSupported=$mDsfidSupported")
Log.d(TAG, "Iso15693Tag: mAfiSupported  =$mAfiSupported")
Log.d(TAG, "Iso15693Tag: mIcRef         =$mIcRef")

mType = "SLIX2"



--------------------

programTag() {
try {    
iCodeTag.connect()
val readWriteBlock = iCodeTag.getRandomNumber() val xorPwd = Utils.xor(Utils.append(readWriteBlock, readWriteBlock)!!, byteArrayOf(0, 0, 0, 0)) iCodeTag.setPasswordRead(xorPwd) iCodeTag.setPasswordWrite(xorPwd) }catch (e: IOException) { e.printStackTrace() Log.e("Activity", "Exception: ", e) } }
ラベル(1)
タグ(4)
0 件の賞賛
返信
1 返信

2,687件の閲覧回数
jimmychan
NXP TechSupport
NXP TechSupport

According to the datasheet 9.5.3.1 GET RANDOM NUMBER, the request format is:

pastedImage_1.png

0 件の賞賛
返信