ICODE SLIX2 Reading Hole

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ICODE SLIX2 Reading Hole

2,091 Views
naokiokazaki
Contributor I

Hi, Team

 

Could someone help me the reason why I had a trouble of reading hole with ICODE SLIX2?

We have developed a new Tag with ICODE SLIX2 which showed better read range compared to ICODE SLI.

However, I saw an issue of the reading hole (null point) at the distance close to a reader antenna and as moving

it away from the reader antenna, it is no problem, we can get UID perfectly .

I did not see such a symptom with ICODE SLI.

 

Best regards,

 

NA

0 Kudos
Reply
2 Replies

1,694 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi NA,

This should be a antenna design issue, please kindly check the antenna design on ICODE SLIX2 side, especially the antenna matching. Please refer to the following link for more details.

http://cache.nxp.com/documents/application_note/AN11180.pdf?fsrch=1&sr=1&pageNum=1


Hope that helps,
Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,694 Views
naokiokazaki
Contributor I

Hi! Kan

Thank you for your input.

However, this is th case of HF, not UHF which you showed here.

I am afraid that the event is different between two.

Best regards,

NA

0 Kudos
Reply