How to unlock PN7462?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to unlock PN7462?

ソリューションへジャンプ
3,065件の閲覧回数
jayesh_joshi
Contributor IV

Hi,

I am using the PN7462AU controller for NFC data transfer. I have downloaded firmware at 0x20A000 instead of 0x203000. After that I am trying to flash code at 0x203000 it is generating an error every time. I have tried erasing flash also but no success. This happens on two separate boards so the issue is critical. 

Thanks, Jayesh.

タグ(3)
0 件の賞賛
返信
1 解決策
3,053件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi Jayesh,

 

Hope you are doing well. Could you please try to update the flash via USB Mass Storage Device interface? Section 8.10 of this User Manual.

 

Hope this helps.

 

Best Regards,

Ricardo

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,021件の閲覧回数
jayesh_joshi
Contributor IV

Thanks @nxf58474 Ricardo

0 件の賞賛
返信
3,054件の閲覧回数
nxf58474
NXP Employee
NXP Employee

Hi Jayesh,

 

Hope you are doing well. Could you please try to update the flash via USB Mass Storage Device interface? Section 8.10 of this User Manual.

 

Hope this helps.

 

Best Regards,

Ricardo

0 件の賞賛
返信