How to get libphhalRf_armcc.lib source code of PN7462?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get libphhalRf_armcc.lib source code of PN7462?

2,323件の閲覧回数
onlineit
Contributor II

How to get libphhalRf_armcc.lib source code of PN7462?

ラベル(2)
0 件の賞賛
返信
4 返答(返信)

2,140件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Xia Shuang,

Why do you need the source code? The lib version should be ok for application development.


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,140件の閲覧回数
onlineit
Contributor II

Hi Kan

     I want to debug the lowerst layer code,all GPIO and AUX and SPI port are redefined in by application development.

    Tks.

    shuang

0 件の賞賛
返信

2,140件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Shuang,

PN7462 has 12 GPIOs , 1 SPIM port and AUX pins , but each of them is fixed to some pin of the device, so I don't understand what you mean for "all GPIO and AUX and SPI port are redefined". Please kindly clarify.

Thanks for your patience!


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,140件の閲覧回数
onlineit
Contributor II

Hi Kan,

          PN7462‘s GPIO is not enough,I would like to use the following SPIM and AUX PINs as GPIOs:

CLK_AUX 2 auxiliary card contact clock/GPIO14
IO_AUX 3 auxiliary card contact I/O/GPIO15
INT_AUX 4 auxiliary card contact interrupt/GPIO16

 

SPIM_SSN 60 SPI master select 1 output/GPIO17
SPI_SCLK 61 SPI master clock output/GPIO18
SPIM_MOSI 62 SPI master data output/GPIO19
SPIM_MISO 63 SPI master data input/GPIO20

Best Regards,

Shuang

0 件の賞賛
返信