Hi @jayesh_joshi ,
Thanks for the information! I just checked with the expert regarding your issue, please kindly refer to the following for details.
This is not really a issue but expected behaviour. Please see UM10858 PN7462 family HW user manual [14.3.3.8 RTS/CTS flow control]:
At the end of the frame reception, the buffer becomes unavailable and the RTS changes to 1 if no other buffer is available, until firmware programs a new buffer.
RTS only will toggle by receiving a EOF. If the RxBuffer is smaller as the receiving frame a buffer overflow interrupt will be generated and data >rxBufferSize will be lost. RTS will be asserted after the frame ended (reception of EOF).
This behaviour cannot be changed.
Best would be to set the rx buffer size bigger as the expected maximum frame size. Multipe rx buffers can be used to operate in a parallel way.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------