How to authenticate MIFARE Plus SE card

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to authenticate MIFARE Plus SE card

4,730 Views
liangjiahua1
Contributor I

Hi,

I use ISO 14443-3 protocol to send “Following authentication” command but get the error code 0x04 (It seems that it means “Block Number out of Range”). Please see below detail:

PCD send: 0x76 0x04 0x40 0x71 0xD6

PICC respond: 0x04

Note: “0x04 0x40” is the AES Sector Keys for Key A for sector 2, LSB first.

What is wrong with it?

0 Kudos
Reply
3 Replies

3,671 Views
xiongqinghua
Contributor I

I have the same question!!!

0 Kudos
Reply

3,671 Views
Kan_Li
NXP TechSupport
NXP TechSupport

You have to request the export control version of NFC reader library from the docstore. Please refer to the following for details.

pastedImage_1.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

3,668 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Liang Jiahua,

We have documentation for this topic, but you have to request it from docstore.nxp.com. Please kindly refer to the attachment for more details.

Hope that helps,

Best regards,

Kan

0 Kudos
Reply