How to authenticate MIFARE Plus SE card

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to authenticate MIFARE Plus SE card

4,766件の閲覧回数
liangjiahua1
Contributor I

Hi,

I use ISO 14443-3 protocol to send “Following authentication” command but get the error code 0x04 (It seems that it means “Block Number out of Range”). Please see below detail:

PCD send: 0x76 0x04 0x40 0x71 0xD6

PICC respond: 0x04

Note: “0x04 0x40” is the AES Sector Keys for Key A for sector 2, LSB first.

What is wrong with it?

0 件の賞賛
返信
3 返答(返信)

3,707件の閲覧回数
xiongqinghua
Contributor I

I have the same question!!!

0 件の賞賛
返信

3,707件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

You have to request the export control version of NFC reader library from the docstore. Please refer to the following for details.

pastedImage_1.png


Have a great day,
Kan

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,704件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi Liang Jiahua,

We have documentation for this topic, but you have to request it from docstore.nxp.com. Please kindly refer to the attachment for more details.

Hope that helps,

Best regards,

Kan

0 件の賞賛
返信